2022-04-11 7:56 AM
Hi all,
I would like to ask if there is a suggested procedure to move the network weights, the one generated inside network_data.h, to external memory-mapped QSPI FLASH.
I've already moved both input/output data and activation to external SRAM, but I'm facing with a compile time error when I do the same with weights (initializer element is not constant).
Before start changing things to solve it, maybe someone of you can help!
I've analysed the example FP-AI-VISION1, but it seems to move only input/output data and activations, not weights.
Thank you and kind regards.
Solved! Go to Solution.
2022-04-11 9:28 AM
Swear I saw a similar question the other week, search here is totally useless
Some related
https://community.st.com/s/question/0D53W00000pReAPSA0/validation-model-failed-to-build-on-cube-ide
2022-04-11 8:25 AM
Ok, sorry, I've missed the definition at the head of FP-AI-VISION1, network_data.h, file:
#if WEIGHT_QSPI == 1 && WEIGHT_QSPI_PROGED == 0
#if defined ( __ICCARM__ )
#pragma location="ExtQSPIFlashSection"
__root /* force linker to keep variable */
#elif defined ( __CC_ARM ) || ( __GNUC__ )
__attribute__((section(".ExtQSPIFlashSection"), used))
#endif
#endif
I will add the section to the linker file and keep you posted.
If you have any other suggestion I thank you in advance.
2022-04-11 9:28 AM
Swear I saw a similar question the other week, search here is totally useless
Some related
https://community.st.com/s/question/0D53W00000pReAPSA0/validation-model-failed-to-build-on-cube-ide
2022-04-13 2:17 AM
Thank you so much for your reply Tesla.
The solution proposed by the FP-AI-VISION1 works very well.