User Activity

In former CubeMX versions an Clock to ADC of 400MHz was possibleNow I am working on CubeMX V 6.3.0 with STM32Cube FW_H7 V1.9.0.The maximum Clock frequency I can adjust is now 79MHz (selected clock source is the PLL2) What is the meaning of the "79 to...
Here definition from the datasheet, but in the 32pin package there is no VDDA !Is any VSS also the VSSA ?
Posted on October 11, 2017 at 15:09In summer 2017, I started an project with the STM32F767 on the Nucleo board, because the H743 was still announced but not available. For some weeks I got the new Nucleo board of the STM32H743. After I transferred t...
Posted on September 29, 2017 at 15:22Is there a bug in the HAL driver lib FW 1.1.0 ?Because SPI4 is not supported.In the routine HAL_SPI_TransmitReceive there is a question'if (IS_SPI_HIGHEND_INSTANCE(hspi->Instance)) ...'the else branch is empty/no...
Kudos from