Posted on March 01, 2018 at 09:08I need to select CAN 2.0 controller in my application.I would like to get low cost evaluation board for the same.Please suggest me STM32 CAN2.0 board so that I can learn CAN.
Posted on September 27, 2017 at 09:08Hi, I am newbie to STM32 controllers.I have to select controller as per following spects.1.Ethernet interface.2.USB interface 4G module3.SD card SPI interface.4.UART interface.6.i2c interface.I need to get dat...
Posted on March 02, 2018 at 07:38i would prefer to get Nucleo-144 as having debugger on board.I have gone through them.Almost 20 types of nucleo-144 board are available.I need Ethernet connector,USB,I2C,SPI,CAN.I have selected NUCLEO-F446ZE.But dat...
Posted on March 01, 2018 at 11:11I dont have to select controller.Controller that i select may not have evaluation board.rather i would select evaluation board having CAN,I2C,SPI interfcace
Posted on March 01, 2018 at 09:15http://www.st.com/en/microcontrollers/stm32f429zi.html board is there but it has LCD.I don't have to use LCD in my app.