cancel
Showing results for 
Search instead for 
Did you mean: 

Please suggest me STM32 CAN2.0 board

Akshay Bhavsar
Associate II
Posted on March 01, 2018 at 09:08

I need to select CAN 2.0 controller in my application.I would like to get low cost evaluation board for the same.

Please suggest me STM32 CAN2.0 board so that I can learn CAN.

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Akshay Bhavsar
Associate II
Posted on March 01, 2018 at 09:15

http://www.st.com/en/microcontrollers/stm32f429zi.html

board is there but it has LCD.I don't have to use LCD in my app.
Imen.D
ST Employee
Posted on March 01, 2018 at 10:52

Hello

akshaybhavsar30

,

I recommend you to use the '

http://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-utilities/st-mcu-finder.html

' tool , it will help you to find the

STM32 microcontrollers which may answer your request.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Akshay Bhavsar
Associate II
Posted on March 01, 2018 at 11:11

I dont have to select controller.Controller that i select may not have evaluation board.rather i would select evaluation board having CAN,I2C,SPI interfcace

Posted on March 01, 2018 at 14:55

You don't have to use the LCD unless you need too. The STM32F429I-DISCO is probably a poor choice for other reasons, including the lack of pins in escape other interfaces. The Nucleo-144 boards offer more opportunity to add your own circuitry and interfaces.

ST's EVAL series boards provide CAN interface(s)

This board using the F107 provides for two

https://www.ebay.com/itm/STM32-ARM-Cortex-M3-STM32F107VCT6-Development-Board/172257169142

 

as does the

https://www.ebay.com/itm/RedDragon407-STM32F4-Cortex-M4-3-2-Ethernet-wireless-2-4G-SDIO-Serial-camera/121087293812

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Akshay Bhavsar
Associate II
Posted on March 01, 2018 at 15:24

Does cortex m3 board has debugger on board?

Posted on March 01, 2018 at 15:32

Both cited boards have a 20-pin JTAG connector, you'll need to use an external pod, either a stand-alone ST-LINK, or pin wiring to one onboard a DISCO or NUCLEO board.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on March 01, 2018 at 15:36

please send me link for ST link debugger

Posted on March 01, 2018 at 15:42

Could you try Google?

http://www.st.com/en/development-tools/st-link-v2.html

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Akshay Bhavsar
Associate II
Posted on March 02, 2018 at 07:38

i would prefer to get Nucleo-144 as having debugger on board.I have gone through them.Almost 20 types of nucleo-144 board are available.I need Ethernet  connector,USB,I2C,SPI,CAN.I have selected NUCLEO-F446ZE.But datasheet says ethernet connector is available depensing on STM32 support.What does that mean?