User Activity

I have been developing firmware for a few years using STM32CubeIDE v1.8.0.  I've been using the STLINK-V3MINI, which has been disconnected.  I've since been using the STLINK-V3MINIE.  I have had some issues with these.  I recently updated the firmwar...
What is the maximum electrical drive frequency that the ST provided firmware can achieve with the STSPIN32F0B IC?  And/or maximum RPM for a 5 pole pair motor?And the same question for the STPIN32G4....For a target frequency of about 1.5 kHz, what wou...
When using STM32CubeIDE, it is easy to inadvertantly make changes to source files that are up on the screen, often as a result of the focus being on the wrong window when one types. (This can easily happen when debugging, e.g. I have the focus on a ...
I have intermittent problems in STM32CubeIDE 1.8.0 opening a .ioc file. When I double click on the file in the Project Explorer, I get a progress bar titled "Loading IOC". When things are working well, as soon as that bar fills up, it is replaced w...
I have a project in a workspace in STM32CubeIDE, generated with STM32CubeMX. I would like to duplicate the entire project, including the .ioc information, to use as the starting point for a new project. How can I do this? I am amazed that this top...