User Activity

 I can't increase the motor speed beyond a certain point.For example, when using the ST Motor Pilot interface, I set the Speed Reference variable to 2500 RPM, and the Mechanical Speed reaches approximately the same value (2495 RPM). However, when I i...
Hi.. We are trying to control a 3-phase asynchronous motor. At first, I used Nucleo STM32G431RB MCU and STEVAL-IHM023V3 board to realize this project, as well as available sample code from ST Motor Control Workbench, version 5.Y.0 (ACIM-NUCLEOG431RB-...
Hi..I am trying to drive an ACIM motor on a project with STEVAL-IHM023V3 using Nucleo STM32G431RB MCU, but in some cases when starting the motor, a phase explodes and Rshunt ,IGBT, driver ,(sometimes) Nucleo STM32G431RB are destroyed.I did some resea...
Kudos from