All the STM32 microcontrollers have the capability to boot from:main flash memory, usually where your firmware is located: at the default value address 0x80000000 or a value define in option byte (if possible).ST embedded bootloader located in the sy...
FAT FS, And I've confusionCommands and response are transmitted as 1 bytes to SD card, so if I initialize SPI using DMA by default each 1 bytes commands/response will be exchanged using DMA method, this will have a overhead of initializing the DMA st...
Thanks for getting out from STM32WB55 zigbee server issue. Do you know how can we registered ourself in https://curiousdesire.com/types-of-backing-storage/ through which we integrated API ourself in our web application?