User Activity

I just set up a new laptop and installed the Cube Programmer but I keep getting the error: CubeProgrammer_API or one of it's dependencies is missing. Please try reinstalling the program or check your java architecture.I am running Windows 10 64-bitI...
I'm trying to program the option bytes on an STM32G0B1 but it keeps timing out at the end of the program sequence and never actually succeeds, no matter how many times I try.I enable the Flash peripheralI (successfully) unlock the flashI (successfull...
The system memory boot mode document (AN2606) states that the G0 uses FDCAN1. However, the reference manual (RM0444) states that it uses FDCAN2... Which one does the boot loader actually use?
The system memory boot mode document (AN2606) states that the G0 uses FDCAN1. However, the reference manual (RM0444) states that it uses FDCAN2... Which one does the boot loader actually use?
Ok, I'm at a complete loss here so I'm looking for any ideas or suggestions. We have a code base that runs on top of FreeRTOS and we have versions of the code that run on multiple, different STM32L4s and on the STM32H753. I ported the code base to ...
Kudos from