Hi There,I am having an issue where I cannot disable Read/Write Protection in the option bytes using ST-LINK. Every time I try to disable it for both banks (uncheck the checkboxes and hit apply) I get the following error:Could not set Option bytes!Pl...
Hi there, I see in the datasheet for various STM32 devices that they support IEEE 1588 PTP.I can't find any options in CubeMX to enable this, and I cant find any HAL code for it.How do I go about setting up IEEE 1588 PTP on a STM32 device?Thanks!
Hi there,I would like to customize the linker script generated by CubeMX.Right now, any changes to the linker file get overwritten when I generate code from CubeMX.Is there a way I can accomplish this? Thanks!
Hi There,I am trying to run the ethernet example from the 1.7.0 version of the STM32H7 firmware at STM32Cube_FW_H7_V1.7.0\Projects\NUCLEO-H743ZI\Applications\LwIP\LwIP_HTTP_Server_Netconn_RTOS.The only modifications I have performed from the provided...
I was able to fix this using the command line interface.First I enabled RDP level 1 with DMEPA. DMEPB, DMESA, DMESB enabled:ST-LINK_CLI.exe -c -OB RDP=1 DMEPA=1 DMEPAB=1 DMESA=1 DEMESB=1Then I switched back to RDP level 0 and set the address ranges t...
Ok I got the nucleo dev board at 1.8V running the LwIP_HTTP_Server_Netconn_RTOS example by enabling HSLV and compensation correction. That was the piece I was missing.Wish the Nucleo reference manual mentioned something about that. Hope this helps so...