cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F3: USB Vendor Class?

Prasant J
Associate III
Posted on June 14, 2017 at 12:20

Hi,

I'm using STM32F303VB in my custom hardware that has USB.

When using STM32CubeMX I see a lot of Standard USB Device classes that I can use (Audio Class, HID, Custom HID,.. etc..). But I do not see an option for Vendor class.(Class code 0xFF) ?

My project requires simple USB communication and I don't want to support standard class protocols. Is there a way by which I can have vendor class in my project?

Any inputs will be of help.

Regards, Prasant

#stm32f303vb #stm32 #usb #usb-vendor-class
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
sibufavica sibufavica
Associate II
Posted on March 24, 2018 at 08:25

Hello Prasant,

Were you able to finish this project? I have the same question. CubeMX doesn't seem to provide USB custom class code generation support. Would like to know if you are able to find a solution.