User Activity

OK, first, I'm not including code quite yet because I want to see if anyone has heard of this problem.  Code is available, though.What I want:  USART to act as a console USART driving a queue for reception, and being fed by a queue for transmission.D...
This has been a long standing problem.If Azure is installed once (on this system), then for search paths in project properties, it is always present.If EmDOS has ever been tried, even though it is not selected and has been removed.  The EmDOS library...
Start a project with FreeRTOS. (default settings_Change your mind and select emDOS. (default settings)build project and get missing variables.  Decide that bug for emDOS is not yet fixed.deselect emDOSSelect FreeRTOS instead.build project (basic, cha...
FreeRTOS is currently at 11.0.  The version in CubeMXIDE is 10.3.1.  There are some good features in 11.0 I'd like to use, so the following questions:11.0 is supposed to be a drop in replacement for 10.6.1  I'd do a download, unzip the files, and jus...
Once emdos has been selected, while the selection can be changed and emdos can be deselected:  The program always puts in a library.  I:LibosT8MLVHLSP.a  Since this file does not exist, compilation fails.  Processor selection is L562Library path adde...
Kudos given to