User Activity

We use HSE osc instead of xtal as suggested by errata. However to support STANDBY we need to turn it off by GPIO. The idea is to boot from SPINAND on HSI and turn HSE in bootloader.Unfortunately it seems that ROM hangs when HSE is not present:< @ 006...
Hello, there is posibility we mixed STM8L101F3 vs F3U. There is marking L1S3 on the top, but I can't find any information/table of these markings. Is is possible to have it ?
In DS12712 Rev 2 (STM32G473) table 13 shows PB10/11 as CAN3_TXFD/CAN3_RXFD but in table 12 CAN is not listed for these pins. Also in tab 13 sometimes it is CAN3_TX and sometimes CAN3_TXFD. Which one is valid ? Interestingly in STM32G474 tab 13 both C...
We have own MP157 based module and it sometimes hangs after NRST during debug. It doesn't respond to JTAG DAP, further NRST pulses doesn't help but NRST_CORE helps. It seems as errata "Incorrect reset of glitch-free kernel clock switch". We tried sw ...
In RM it is stated that in Engineering mode (BOOT pins at 3'b100) the MPU re-opens CA7 secure debug.I boot in that mode, then halt in openocd:stm32mp15x.cpu0: hardware has 6 breakpoints, 4 watchpoints > halt stm32mp15x.cpu0 rev 5, partnum c07, arch f...
Kudos from