User Activity

Environment:MacOS 10.14.6STM32CubeIDE 1.6.1STM32WB SDK 1.11.0Starting with a clean install of Cube, SDK, empty workspace. Importing p2p_Server project (from the initial splash screen->Import STM32 sample app), the build fails with (among other):/Use...
The documentation for STM32WB55 Nucleo states that a 5.2 stack is available ("comes with") but the BT stack provided in STM32Cube_FW_WB_V1.11.0 is a 5.0 stack...Regards,AC
As the title says. I can see no support for this but a perpiheral advertising with ADV_IND should support this by default.Does anyone know?Regards,AC
Hi,I have a STM32WB55-Nucleo running the BLE_HeartRateFreeRTOS sample application. All works well for a while - I can scan and connect to it (from LightBlue on iOS) and read, write and subscribe to notifications. However, after approximately 40 mins,...
Documentation says that the BlueNRG-LP is certified for Bluetooth 5.2 but it does not make mention of isochronous channels/LE Audio support. Is LE Audio supported? Is there a stack that supports LE Audio?Regards,AC