2021-04-13 5:29 AM
Environment:
MacOS 10.14.6
STM32CubeIDE 1.6.1
STM32WB SDK 1.11.0
Starting with a clean install of Cube, SDK, empty workspace. Importing p2p_Server project (from the initial splash screen->Import STM32 sample app), the build fails with (among other):
/Users/skajam66/Developer/stm/workspace/BLE_p2pServer/STM32_WPAN/App/app_ble.c:517:11: error: 'handleNotification' undeclared (first use in this function); did you mean 'HRS_Notification'?
517 | handleNotification.P2P_Evt_Opcode = PEER_CONN_HANDLE_EVT;
| ^~~~~~~~~~~~~~~~~~
| HRS_Notification
/Users/skajam66/Developer/stm/workspace/BLE_p2pServer/STM32_WPAN/App/app_ble.c:517:11: note: each undeclared identifier is reported only once for each function it appears in
/Users/skajam66/Developer/stm/workspace/BLE_p2pServer/STM32_WPAN/App/app_ble.c:517:47: error: 'PEER_CONN_HANDLE_EVT' undeclared (first use in this function); did you mean 'HIDS_CONN_HANDLE_EVT'?
517 | handleNotification.P2P_Evt_Opcode = PEER_CONN_HANDLE_EVT;Adding an include statement in app_ble.c:
#include "p2p_server_app.h"gets rid of the second error. Adding a handleNotification variable:
/* USER CODE BEGIN PTD */
P2PS_APP_ConnHandle_Not_evt_t handleNotification;
/* USER CODE END PTD */gets rid of the first error but now throws up multiple linker errors:
app_ble.c:519: undefined reference to `P2PS_APP_Notification'
app_ble.c:637: undefined reference to `P2PS_APP_SW1_Button_Action'
p2p_stm.c:139: undefined reference to `P2PS_STM_App_Notification'All of these symbols are implemented in p2p_server_app.c which is not getting compiled. Both p2p_server_app.c and p2p_server_app.h are in the same build directory as app_ble.c but p2p_server.c is not being compiled.
Is there a configuration setting that I am missing? Seems odd that a core source file for BLE_Server is not getting picked up.
Regards,
ac