cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to debug the STM32MP157 with ST-Link? I have the STM32MP157A-DK1, and am working with a VirtualBox Ubuntu system with the CubeIDE. We really do not want an ethernet port on our final product.

MDoxb.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
KnarfB
Principal III

There are many different levels on debugging possible on STM32MP157, here is an overview: https://wiki.st.com/stm32mpu/wiki/STM32MP1_Platform_trace_and_debug_environment_overview

In a final product, you won't do typical bring-up tasks close to hardware and schematics level but rather want Linux debugging tools for developing/updating at the Linux file/application/kernel level.

Network access could be done via an external USB/Ethernet adapter on an USB port if you prefer.

Check also AN5031Application note for HW development.

hth

KnarfB