I use FSMC in STM32F407 to access external SRAM IS62WV51216. I read RM0090 and AN2784, gives me two fomulatSU means here is the timing graphhere is write timing graphwhy WE have two falling edges on the leftwhat dose tSU tV mean,where is it in the t...
I am from China,I was told that STM32 hardware I2C has bug.So I always use software simulation I2C with two ordinary GPIO Pins. I was wondering what is the bug exactly?Is it a rumor ,or is it true?I hope get opinion from abroad website,because you sp...
I am simulating stm32f103c6 in proteus,I want to do timer2 interrupt ,I set pre = 7200-1,psc = 10000-1,so 1s to timer2 update interrupt.But time is not correct,it does not work.I look up information,it is said I need to change stm32 clk to 8MHz,not...