Skip to main content
Ethan1
Associate II
July 12, 2024
Question

stdlib bug - STM32F4 SPL (Standard Peripheral Library)

  • July 12, 2024
  • 5 replies
  • 1792 views

in stdlib version1.9.0,

 

void I2S_Init(SPI_TypeDef* SPIx, I2S_InitTypeDef* I2S_InitStruct)
{
 uint16_t tmpreg = 0, i2sdiv = 2, i2sodd = 0, packetlength = 1;
 uint32_t tmp = 0, i2sclk = 0;
#ifndef I2S_EXTERNAL_CLOCK_VAL
 uint32_t pllm = 0, plln = 0, pllr = 0;
#endif /* I2S_EXTERNAL_CLOCK_VAL */
 
 /* Check the I2S parameters */
 assert_param(IS_SPI_23_PERIPH(SPIx));
 assert_param(IS_I2S_MODE(I2S_InitStruct->I2S_Mode));
 assert_param(IS_I2S_STANDARD(I2S_InitStruct->I2S_Standard));
 assert_param(IS_I2S_DATA_FORMAT(I2S_InitStruct->I2S_DataFormat));
 assert_param(IS_I2S_MCLK_OUTPUT(I2S_InitStruct->I2S_MCLKOutput));
 assert_param(IS_I2S_AUDIO_FREQ(I2S_InitStruct->I2S_AudioFreq));
 assert_param(IS_I2S_CPOL(I2S_InitStruct->I2S_CPOL)); 

/*----------------------- SPIx I2SCFGR & I2SPR Configuration -----------------*/
 /* Clear I2SMOD, I2SE, I2SCFG, PCMSYNC, I2SSTD, CKPOL, DATLEN and CHLEN bits */
 SPIx->I2SCFGR &= I2SCFGR_CLEAR_MASK; 
 SPIx->I2SPR = 0x0002;
 
 /* Get the I2SCFGR register value */
 tmpreg = SPIx->I2SCFGR;
 
 /* If the default value has to be written, reinitialize i2sdiv and i2sodd*/
 if(I2S_InitStruct->I2S_AudioFreq == I2S_AudioFreq_Default)
 {
 i2sodd = (uint16_t)0;
 i2sdiv = (uint16_t)2; 
 }
 /* If the requested audio frequency is not the default, compute the prescaler */
 else
 {
 /* Check the frame length (For the Prescaler computing) *******************/
 if(I2S_InitStruct->I2S_DataFormat == I2S_DataFormat_16b)
 {
 /* Packet length is 16 bits */
 packetlength = 16;
 }
 else
 {
 /* Packet length is 32 bits */
 packetlength = 32;
 }

 if(I2S_InitStruct->I2S_Standard <= I2S_Standard_LSB)
 {
 /* In I2S standard packet length is multiplied by 2 */
 packetlength = packetlength * 2;
 }

 /* Get I2S source Clock frequency ****************************************/
 
 /* If an external I2S clock has to be used, this define should be set 
 in the project configuration or in the stm32f4xx_conf.h file */
 #ifdef I2S_EXTERNAL_CLOCK_VAL 
 /* Set external clock as I2S clock source */
 if ((RCC->CFGR & RCC_CFGR_I2SSRC) == 0)
 {
 RCC->CFGR |= (uint32_t)RCC_CFGR_I2SSRC;
 }
 
 /* Set the I2S clock to the external clock value */
 i2sclk = I2S_EXTERNAL_CLOCK_VAL;

 #else /* There is no define for External I2S clock source */
 /* Set PLLI2S as I2S clock source */
 if ((RCC->CFGR & RCC_CFGR_I2SSRC) != 0)
 {
 RCC->CFGR &= ~(uint32_t)RCC_CFGR_I2SSRC;
 } 
 
 /* Get the PLLI2SN value */
 plln = (uint32_t)(((RCC->PLLI2SCFGR & RCC_PLLI2SCFGR_PLLI2SN) >> 6) & \
 (RCC_PLLI2SCFGR_PLLI2SN >> 6));
 
 /* Get the PLLI2SR value */
 pllr = (uint32_t)(((RCC->PLLI2SCFGR & RCC_PLLI2SCFGR_PLLI2SR) >> 28) & \
 (RCC_PLLI2SCFGR_PLLI2SR >> 28));
 
 /* Get the PLLM value */
 pllm = (uint32_t)(RCC->PLLCFGR & RCC_PLLCFGR_PLLM);

 if((RCC->PLLCFGR & RCC_PLLCFGR_PLLSRC) == RCC_PLLCFGR_PLLSRC_HSE)
 {
 /* Get the I2S source clock value */
 i2sclk = (uint32_t)(((HSE_VALUE / pllm) * plln) / pllr);
 }
 else
 { /* Get the I2S source clock value */
 i2sclk = (uint32_t)(((HSI_VALUE / pllm) * plln) / pllr);
 }
 #endif /* I2S_EXTERNAL_CLOCK_VAL */
 
 /* Compute the Real divider depending on the MCLK output state, with a floating point */
 if(I2S_InitStruct->I2S_MCLKOutput == I2S_MCLKOutput_Enable)
 {
 /* MCLK output is enabled */
 tmp = (uint16_t)(((((i2sclk / 256) * 10) / I2S_InitStruct->I2S_AudioFreq)) + 5);
 }
 else
 {
 /* MCLK output is disabled */
 tmp = (uint16_t)(((((i2sclk / (32 * packetlength)) *10 ) / I2S_InitStruct->I2S_AudioFreq)) + 5);
 }
 
 /* Remove the flatting point */
 tmp = tmp / 10; 
 
 /* Check the parity of the divider */
 i2sodd = (uint16_t)(tmp & (uint16_t)0x0001);
 
 /* Compute the i2sdiv prescaler */
 i2sdiv = (uint16_t)((tmp - i2sodd) / 2);
 
 /* Get the Mask for the Odd bit (SPI_I2SPR[8]) register */
 i2sodd = (uint16_t) (i2sodd << 8);
 }

 /* Test if the divider is 1 or 0 or greater than 0xFF */
 if ((i2sdiv < 2) || (i2sdiv > 0xFF))
 {
 /* Set the default values */
 i2sdiv = 2;
 i2sodd = 0;
 }

 /* Write to SPIx I2SPR register the computed value */
 SPIx->I2SPR = (uint16_t)((uint16_t)i2sdiv | (uint16_t)(i2sodd | (uint16_t)I2S_InitStruct->I2S_MCLKOutput));
 
 /* Configure the I2S with the SPI_InitStruct values */
 tmpreg |= (uint16_t)((uint16_t)SPI_I2SCFGR_I2SMOD | (uint16_t)(I2S_InitStruct->I2S_Mode | \
 (uint16_t)(I2S_InitStruct->I2S_Standard | (uint16_t)(I2S_InitStruct->I2S_DataFormat | \
 (uint16_t)I2S_InitStruct->I2S_CPOL))));
 
#if defined(SPI_I2SCFGR_ASTRTEN)
 if((I2S_InitStruct->I2S_Standard == I2S_Standard_PCMShort) || (I2S_InitStruct->I2S_Standard == I2S_Standard_PCMLong))
 {
 /* Write to SPIx I2SCFGR */ 
 SPIx->I2SCFGR = tmpreg | SPI_I2SCFGR_ASTRTEN;
 }
#else
 /* Write to SPIx I2SCFGR */ 
 SPIx->I2SCFGR = tmpreg ;
#endif 
}

 

in older version,the same function is

 

void I2S_Init(SPI_TypeDef* SPIx, I2S_InitTypeDef* I2S_InitStruct)
{
 uint16_t tmpreg = 0, i2sdiv = 2, i2sodd = 0, packetlength = 1;
 uint32_t tmp = 0, i2sclk = 0;
#ifndef I2S_EXTERNAL_CLOCK_VAL
 uint32_t pllm = 0, plln = 0, pllr = 0;
#endif /* I2S_EXTERNAL_CLOCK_VAL */
 
 /* Check the I2S parameters */
 assert_param(IS_SPI_23_PERIPH(SPIx));
 assert_param(IS_I2S_MODE(I2S_InitStruct->I2S_Mode));
 assert_param(IS_I2S_STANDARD(I2S_InitStruct->I2S_Standard));
 assert_param(IS_I2S_DATA_FORMAT(I2S_InitStruct->I2S_DataFormat));
 assert_param(IS_I2S_MCLK_OUTPUT(I2S_InitStruct->I2S_MCLKOutput));
 assert_param(IS_I2S_AUDIO_FREQ(I2S_InitStruct->I2S_AudioFreq));
 assert_param(IS_I2S_CPOL(I2S_InitStruct->I2S_CPOL)); 

/*----------------------- SPIx I2SCFGR & I2SPR Configuration -----------------*/
 /* Clear I2SMOD, I2SE, I2SCFG, PCMSYNC, I2SSTD, CKPOL, DATLEN and CHLEN bits */
 SPIx->I2SCFGR &= I2SCFGR_CLEAR_MASK; 
 SPIx->I2SPR = 0x0002;
 
 /* Get the I2SCFGR register value */
 tmpreg = SPIx->I2SCFGR;
 
 /* If the default value has to be written, reinitialize i2sdiv and i2sodd*/
 if(I2S_InitStruct->I2S_AudioFreq == I2S_AudioFreq_Default)
 {
 i2sodd = (uint16_t)0;
 i2sdiv = (uint16_t)2; 
 }
 /* If the requested audio frequency is not the default, compute the prescaler */
 else
 {
 /* Check the frame length (For the Prescaler computing) *******************/
 if(I2S_InitStruct->I2S_DataFormat == I2S_DataFormat_16b)
 {
 /* Packet length is 16 bits */
 packetlength = 1;
 }
 else
 {
 /* Packet length is 32 bits */
 packetlength = 2;
 }

 /* Get I2S source Clock frequency ****************************************/
 
 /* If an external I2S clock has to be used, this define should be set 
 in the project configuration or in the stm32f4xx_conf.h file */
 #ifdef I2S_EXTERNAL_CLOCK_VAL 
 /* Set external clock as I2S clock source */
 if ((RCC->CFGR & RCC_CFGR_I2SSRC) == 0)
 {
 RCC->CFGR |= (uint32_t)RCC_CFGR_I2SSRC;
 }
 
 /* Set the I2S clock to the external clock value */
 i2sclk = I2S_EXTERNAL_CLOCK_VAL;

 #else /* There is no define for External I2S clock source */
 /* Set PLLI2S as I2S clock source */
 if ((RCC->CFGR & RCC_CFGR_I2SSRC) != 0)
 {
 RCC->CFGR &= ~(uint32_t)RCC_CFGR_I2SSRC;
 } 
 
 /* Get the PLLI2SN value */
 plln = (uint32_t)(((RCC->PLLI2SCFGR & RCC_PLLI2SCFGR_PLLI2SN) >> 6) & \
 (RCC_PLLI2SCFGR_PLLI2SN >> 6));
 
 /* Get the PLLI2SR value */
 pllr = (uint32_t)(((RCC->PLLI2SCFGR & RCC_PLLI2SCFGR_PLLI2SR) >> 28) & \
 (RCC_PLLI2SCFGR_PLLI2SR >> 28));
 
 /* Get the PLLM value */
 pllm = (uint32_t)(RCC->PLLCFGR & RCC_PLLCFGR_PLLM);

 if((RCC->PLLCFGR & RCC_PLLCFGR_PLLSRC) == RCC_PLLCFGR_PLLSRC_HSE)
 {
 /* Get the I2S source clock value */
 i2sclk = (uint32_t)(((HSE_VALUE / pllm) * plln) / pllr);
 }
 else
 { /* Get the I2S source clock value */
 i2sclk = (uint32_t)(((HSI_VALUE / pllm) * plln) / pllr);
 }
 #endif /* I2S_EXTERNAL_CLOCK_VAL */
 
 /* Compute the Real divider depending on the MCLK output state, with a floating point */
 if(I2S_InitStruct->I2S_MCLKOutput == I2S_MCLKOutput_Enable)
 {
 /* MCLK output is enabled */
 tmp = (uint16_t)(((((i2sclk / 256) * 10) / I2S_InitStruct->I2S_AudioFreq)) + 5);
 }
 else
 {
 /* MCLK output is disabled */
 tmp = (uint16_t)(((((i2sclk / (32 * packetlength)) *10 ) / I2S_InitStruct->I2S_AudioFreq)) + 5);
 }
 
 /* Remove the flatting point */
 tmp = tmp / 10; 
 
 /* Check the parity of the divider */
 i2sodd = (uint16_t)(tmp & (uint16_t)0x0001);
 
 /* Compute the i2sdiv prescaler */
 i2sdiv = (uint16_t)((tmp - i2sodd) / 2);
 
 /* Get the Mask for the Odd bit (SPI_I2SPR[8]) register */
 i2sodd = (uint16_t) (i2sodd << 8);
 }

 /* Test if the divider is 1 or 0 or greater than 0xFF */
 if ((i2sdiv < 2) || (i2sdiv > 0xFF))
 {
 /* Set the default values */
 i2sdiv = 2;
 i2sodd = 0;
 }

 /* Write to SPIx I2SPR register the computed value */
 SPIx->I2SPR = (uint16_t)((uint16_t)i2sdiv | (uint16_t)(i2sodd | (uint16_t)I2S_InitStruct->I2S_MCLKOutput));
 
 /* Configure the I2S with the SPI_InitStruct values */
 tmpreg |= (uint16_t)((uint16_t)SPI_I2SCFGR_I2SMOD | (uint16_t)(I2S_InitStruct->I2S_Mode | \
 (uint16_t)(I2S_InitStruct->I2S_Standard | (uint16_t)(I2S_InitStruct->I2S_DataFormat | \
 (uint16_t)I2S_InitStruct->I2S_CPOL))));
 
 /* Write to SPIx I2SCFGR */ 
 SPIx->I2SCFGR = tmpreg;
}

 

Ethan1_0-1720779658564.png

differ as picture above, I think there is a problem. Can you help me with it?

This topic has been closed for replies.

5 replies

ST Employee
July 12, 2024

Hello @Ethan1 ,

The change in packet length calculation seems to be an attempt to correct the prescaler computation for different I2S standards and data formats. The older version might have had issues with certain configurations, leading to incorrect clock settings
Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Ethan1
Ethan1Author
Associate II
July 14, 2024

So you mean now version is better? But old project using old version can work normal, after updating 1.9.0, it does`nt work well.

AScha.3
Super User
July 14, 2024

So change the 

packetlength = 16;
->
packetlength = 1;

and same for ...32 -> 2 ;

then try and tell...

If you feel a post has answered your question, please click on " Best Answer ".
Ethan1
Ethan1Author
Associate II
July 15, 2024

you mean change 16 to 1 32 to 2,and try the program, tell you consequence? English is not my mother tougue