2013-04-07 07:00 PM
2013-04-07 07:06 PM
You can run into a lot of problems with SWD/JTAG connectivity in low power modes.
2013-04-07 07:09 PM
Thanks clive, so you means my code was entered into low power mode?
B.R.Jin2013-04-08 03:55 AM
There are several things you can do in your code that can break ST-LINK connectivity. If the problem is with your code this can be identified by resetting the part with BOOT0 High
2013-04-08 05:50 PM
Yes, it happens when I run the Custom_HID demo code in the debug mode and remove the USB cable.
B.R.Jin