User Activity

Posted on September 19, 2013 at 17:43Hi EverybodyIm power my motor with 22 Volts with the following Register values:KVAL Register 0X10 (HEX) OC SD_ DISABLE = Do not schut down the bridges on overcurrentAs the voltage rises to 24V (in orden to obtain...
Posted on November 30, 2012 at 16:43Hello ST!We are using the L6470 and it is working quite well. But: We have problems when reading the ABS_POS register. It seems to be that the 8th Bit (for 128) is always Low. See Our values:   Go To Pos   R...