cancel
Showing results for 
Search instead for 
Did you mean: 

24 Volts Power Supply_Causes Error_Motor Stop

edgar23
Associate II
Posted on September 19, 2013 at 17:43

Hi Everybody

Im power my motor with 22 Volts with the following Register values:

KVAL Register 0X10 (HEX) 

OC SD_ DISABLE = Do not schut down the bridges on overcurrent

As the voltage rises to 24V (in orden to obtain more Torque)  the engine stops and lose its Torque.. I Just need to power again  with 22V  and the motor works 

Anybody knows what im doing wrong.. Why stops the motor exactly on 24 V?

Thank you for your help

#l6470-24-volts_-motor-stop
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Gigi
ST Employee
Posted on January 02, 2014 at 10:17

CiaoEdgar

I suggest post this thread in the

https://my.st.com/public/STe2ecommunities/motordriver_ics/Lists/Motor%20Driver%20ICs%20and%20Boards/AllItems.aspx

forum.

Thanks

Ciao

Gigi