Hi! While ST doesn't provide anything as complex and all-encompassing like the MCSDK toolsuite for driving PMSM and BLDC motors, there is a selection of X-Cube-SPN(1, 2, 3, 5, 6, and 14) software expansion packages to go with the following X-Nucleo e...
Hello.ST does not provide sources for the 4.0.0+ versions of the library which is delivered as a compiled object code.For G0, however, the older version 2.3.0 version is available, which contains the source code and can be used to build upon or as an...
Hello, there is a directory named uninstaller containing the uninstaller in the STM32CubeProgrammer install directory ( /usr/local/STMicroelectronics/STM32Cube/STM32CubeProgrammer by default ). If your system doesn't automatically execute the java ....
The 31.25 ns is indeed the shortest sampling time possible. The mention of 18.75 ns in the datasheet is indeed an error. My previous reply was incorrect. I apologize for any inconvenience.18.75 ns sampling time is possible, the 31.25 ns is the lowest...