cancel
Showing results for 
Search instead for 
Did you mean: 

Is there an example for the x-cube-azrtos-l4 for winusb

MikeAtETI
Associate III

Is there an example for the x-cube-azrtos-l4 usbx stack showing how to implement the additional string descriptions and GET_OS_FEATURE_DESCRIPTOR features to allow an HID device to appear as WinUSB?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
MikeAtETI
Associate III

To help those who might find by searching, we've made the following modifications and it now shows as WinUSB.

See WCID Devices · pbatard/libwdi Wiki (github.com) for more implementation info

In MX_USBX_Device_Init, after ux_device_stack_class_register and its return check add:

_ux_device_stack_microsoft_extension_register(USB_REQ_GET_OS_FEATURE_DESCRIPTOR, CustomMicrosoftRequestHandler);

The following is the CustomMicrosoftRequestHandler:

#define  CustomHID_TYPE_OS_FEATURE_EXT_PROPERTIES           5
#define  CustomHID_TYPE_OS_FEATURE_EXT_COMPAT_ID            4
 
USBD_CompatIDDescStruct USBD_CompatIDDesc = { sizeof(USBD_CompatIDDesc), 0x0100, 0x0004, 0x01, {0}, 0x00, 0x01, "WINUSB", {0}, {0} };
USBD_ExtPropertiesDescStruct USBD_ExtPropertiesDesc = { sizeof(USBD_ExtPropertiesDescStruct), 0x0100, 0x0005, 0x0001,\
136, 7,\
42,     {'D', 'e', 'v', 'i', 'c', 'e', 'I', 'n', 't', 'e', 'r', 'f', 'a', 'c', 'e', 'G', 'U', 'I', 'D', 's'},\
80, \
{'{', '4', '6', '7', '1', '4', '8', 'F', 'B', '-', '3', 'A', '6', '1', '-', '4', '1', '0', '2', '-', '8', '8', '5', '1', '-', 'B', '1', '3', '5', 'C', '5', '7', '5', '2', '2', '4', '2', '}', 0, 0 } };
 
UINT CustomMicrosoftRequestHandler(ULONG request, ULONG request_value, ULONG request_index, ULONG request_length, UCHAR *pData, ULONG *pApplication_data_length)
{
	if (request == USB_REQ_GET_OS_FEATURE_DESCRIPTOR)
	{
		switch(request_index)
		{
		case CustomHID_TYPE_OS_FEATURE_EXT_COMPAT_ID:
			memcpy(pData, &USBD_CompatIDDesc, sizeof(USBD_CompatIDDescStruct));
			*pApplication_data_length = sizeof(USBD_CompatIDDescStruct);
			return UX_SUCCESS;
			break;
		case CustomHID_TYPE_OS_FEATURE_EXT_PROPERTIES:
			memcpy(pData, &USBD_ExtPropertiesDesc, sizeof(USBD_ExtPropertiesDescStruct));
			*pApplication_data_length = sizeof(USBD_ExtPropertiesDescStruct);
			return UX_SUCCESS;
			break;
		}
	}
	return UX_ERROR;
}

and this is the addition in ux_device_descriptors.c

uint8_t CustomHID_StringWinUSB[18] =  { 0x12, 0x03, 'M',0,'S',0,'F',0,'T',0,'1',0,'0',0,'0',0, USB_REQ_GET_OS_FEATURE_DESCRIPTOR, 0 };

and then add this to USBD_Get_String_Framework:

// Microsoft OS Descriptor
  USBD_string_framework[count++] = USBD_LANGID_STRING & 0xFF;
  USBD_string_framework[count++] = USBD_LANGID_STRING >> 8;
  USBD_string_framework[count++] = 0xEE;
  USBD_Desc_GetString((uint8_t *)CustomHID_StringWinUSB, USBD_string_framework + count, &len);
  count += len + 1;

View solution in original post

4 REPLIES 4
MikeAtETI
Associate III

Looks like you can extend the string descriptors for the extra descriptor extending USBD_Get_String_Framework for the extra string descriptor (0xEE)

There looks to be a function _ux_device_stack_microsoft_extension_register that may be where you hook the function descriptor bits in, but its unclear how to use it.

mohamed.ayed
ST Employee

Hi @MikeAtETI​  We don't provide yet WinUSB example or template in our Azure RTOS packages

MikeAtETI
Associate III

To help those who might find by searching, we've made the following modifications and it now shows as WinUSB.

See WCID Devices · pbatard/libwdi Wiki (github.com) for more implementation info

In MX_USBX_Device_Init, after ux_device_stack_class_register and its return check add:

_ux_device_stack_microsoft_extension_register(USB_REQ_GET_OS_FEATURE_DESCRIPTOR, CustomMicrosoftRequestHandler);

The following is the CustomMicrosoftRequestHandler:

#define  CustomHID_TYPE_OS_FEATURE_EXT_PROPERTIES           5
#define  CustomHID_TYPE_OS_FEATURE_EXT_COMPAT_ID            4
 
USBD_CompatIDDescStruct USBD_CompatIDDesc = { sizeof(USBD_CompatIDDesc), 0x0100, 0x0004, 0x01, {0}, 0x00, 0x01, "WINUSB", {0}, {0} };
USBD_ExtPropertiesDescStruct USBD_ExtPropertiesDesc = { sizeof(USBD_ExtPropertiesDescStruct), 0x0100, 0x0005, 0x0001,\
136, 7,\
42,     {'D', 'e', 'v', 'i', 'c', 'e', 'I', 'n', 't', 'e', 'r', 'f', 'a', 'c', 'e', 'G', 'U', 'I', 'D', 's'},\
80, \
{'{', '4', '6', '7', '1', '4', '8', 'F', 'B', '-', '3', 'A', '6', '1', '-', '4', '1', '0', '2', '-', '8', '8', '5', '1', '-', 'B', '1', '3', '5', 'C', '5', '7', '5', '2', '2', '4', '2', '}', 0, 0 } };
 
UINT CustomMicrosoftRequestHandler(ULONG request, ULONG request_value, ULONG request_index, ULONG request_length, UCHAR *pData, ULONG *pApplication_data_length)
{
	if (request == USB_REQ_GET_OS_FEATURE_DESCRIPTOR)
	{
		switch(request_index)
		{
		case CustomHID_TYPE_OS_FEATURE_EXT_COMPAT_ID:
			memcpy(pData, &USBD_CompatIDDesc, sizeof(USBD_CompatIDDescStruct));
			*pApplication_data_length = sizeof(USBD_CompatIDDescStruct);
			return UX_SUCCESS;
			break;
		case CustomHID_TYPE_OS_FEATURE_EXT_PROPERTIES:
			memcpy(pData, &USBD_ExtPropertiesDesc, sizeof(USBD_ExtPropertiesDescStruct));
			*pApplication_data_length = sizeof(USBD_ExtPropertiesDescStruct);
			return UX_SUCCESS;
			break;
		}
	}
	return UX_ERROR;
}

and this is the addition in ux_device_descriptors.c

uint8_t CustomHID_StringWinUSB[18] =  { 0x12, 0x03, 'M',0,'S',0,'F',0,'T',0,'1',0,'0',0,'0',0, USB_REQ_GET_OS_FEATURE_DESCRIPTOR, 0 };

and then add this to USBD_Get_String_Framework:

// Microsoft OS Descriptor
  USBD_string_framework[count++] = USBD_LANGID_STRING & 0xFF;
  USBD_string_framework[count++] = USBD_LANGID_STRING >> 8;
  USBD_string_framework[count++] = 0xEE;
  USBD_Desc_GetString((uint8_t *)CustomHID_StringWinUSB, USBD_string_framework + count, &len);
  count += len + 1;

Hello,

Thank you for this sample.

But I do not think it will work with USBX. Specifically, if you look at ux_device_stack_descriptor_send(), the part that handles UX_STRING_DESCRIPTOR_ITEM, it assumes that the string framework string value is a ASCII string and converts it to UNICODE. That means CustomHID_StringWinUSB will get extra zeros inserted, which will make it invalid.

I am looking at it, as if it is used directly with USBX.

Thank you,

D.