cancel
Showing results for 
Search instead for 
Did you mean: 

STMVL-Discovery - Target not connected

lastsamurai
Associate III
Posted on May 04, 2011 at 03:19

HI,

I have a problem with STM32VL discovery board.  When I try to connect to the board via SWD through ST-Link utility, I get the message that target is not connected!  But I can connect to the board through ST-Link menu and even can do firmware updates.

Processor seems to be working, as it gives me the outputs of the last program, which I programmed to it. 

Any Ideas?

Cheers,

Sam

#stm32-st-link-utility #st-link
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
lastsamurai
Associate III
Posted on May 06, 2011 at 06:56

Hi,

Was able to connect it through ULink and erase the flash!

Now it is connecting through ST link and works like a charm!