Posted on May 17, 2011 at 13:56Hello, We have made such a system, detecting zero-point with 3x270K resistors from line to pin on uC. This will give squarewave on the input. If you then connect a 10K input pin on the uC, whre the 270k is connected to...
Posted on May 17, 2011 at 13:46Hello,Maybe you could look how the circle_os is made from the Primer2. I think they have a array with pointers to all the functions there is embedded in the OS, this list is as i remember placed fixed after the IRQ vec...
Posted on May 17, 2011 at 13:40Hello, I got it up running in Keil with their TCP/IP stack and dynamic ram allocation. I just need to try to eliminate the need for copy the entire packet as done in the original driver, that is a of time wasted. you c...
Posted on May 17, 2011 at 13:40Hello, Yes i found that library ''WiShield'' if that is the one?.. I allready converted that into my code and properly going to test that today, only need to solder some wires on a ZeroG module to test it. But i think ...
Posted on May 17, 2011 at 13:40 Hello, could you please then share the link/file, because my account only gives access to the electrical datasheet and nothing about the protocol/register/setup etc. Kasper