2009-08-30 4:19 PM
problem of USART's CTS RTS
2011-05-17 4:21 AM
hello,
I meet this problem when using gpio pin PA11 and PA12, this two pins are shared as USART1's CTS and RTS.when sending data on USART1,pulses could be detected on this two pins.However, I didn't enable CTS and RTS.And I have checked the regesiters of USART1 when simulating, they are not enabled indeed. has anyone know the reason? or it is a silicon bug?2011-05-17 4:21 AM
Hi superwht,
Could you detail how did you configured your Pins, PA9, PA10, PA11 and PA12 ? may be you have a wrong configuration in software, or may be also your hardware layout is not clean and external cross-talk is created between pins. Cheers, STOne-32.2011-05-17 4:21 AM
STone-32,
thanks for your advices, I have checked the external circuit and found the problem actually come from the circuit.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.