Posted on May 17, 2011 at 15:03How should unbonded pins be configured? For example, Port H0 is on pin 13 of an STM8S208 in the LQFP80 package, but is not present on the LQFP64 package. Should it be setup as an output with a Data value of ''0'' ? Or ...
Posted on May 17, 2011 at 15:03On page 373 of the STM8S reference manual, in the description of the beCAN Clock System, just below figure 143 it says ''The frequency of the external clock fCANEXT must be less that that of the the CPU clock fCPU.'' W...
Posted on May 17, 2011 at 15:03I would like to run an STM8S208RBT6 from an external 1 Mhz clock. However, it appears that if I do this the ADC cannot be used since the ADC requires at least a 1 MHz clock, and the minimum ADC clock prescale ratio is ...