cancel
Showing results for 
Search instead for 
Did you mean: 

STM8S208 external clock

ptsmith
Associate II
Posted on June 24, 2009 at 08:15

STM8S208 external clock

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
ptsmith
Associate II
Posted on May 17, 2011 at 15:03

I would like to run an STM8S208RBT6 from an external 1 Mhz clock. However, it appears that if I do this the ADC cannot be used since the ADC requires at least a 1 MHz clock, and the minimum ADC clock prescale ratio is /2 from fMASTER.

So, am I correct that in order to use the ADC, the minimum external clock is 2 MHz?

Paul Smith

Indiana University Physics

mozra27
Associate II
Posted on May 17, 2011 at 15:03

Hi Paul,

Yes, you are right the minimum value for fADC is 1MHz can by a prescaled fMASTER clock. The prescaling factor of the clock depends on the SPSEL[2:0] bits in the ADC_CR1 register.

Regards

mozra