cancel
Showing results for 
Search instead for 
Did you mean: 

flash up-date firmware

franco2
Associate II
Posted on October 17, 2007 at 06:30

flash up-date firmware

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
16-32micros
Associate III
Posted on May 17, 2011 at 12:16

Dear Franco,

Yes, this is possible and this Method is called IAP ( In-Application programming) you can choose your preferred Communcation Protocol, here in your case the SPI. There is an example on ST web site using the UART (RS232)

http://www.st.com/stonline/products/literature/an/13588.pdf

and its associated

http://www.st.com/stonline/products/support/micro/files/an2557.zip

that you can tailor to SPI with your preferred memory or using another SPI Device.

Regards, ;)

[ This message was edited by: STOne-32 on 15-10-2007 19:35 ]

franco2
Associate II
Posted on May 17, 2011 at 12:16

Thanks for your information

franco2
Associate II
Posted on May 17, 2011 at 12:16

He at all

In the special application I must use the SPI for up-date the firmware in the STM32F10xxx microcontroller is possiple this?

If yes I must place the code for the SPI function on flash proteted area and read the new data for up-date the firmware from it and after write this new data in flash, is possible this or is correct this procedure?

Exsiting a sample of the code for implement this?

Franco