Posted on May 17, 2011 at 09:44Try changing the bit timing In 91x_can.c if have changed the line: CAN_TIMING(11, 4, 4, 4), /*0x3AC3 125 kbit/s 16 11 4 4 4 */ to: CAN_TIMING(13, 5, 4, 40), /*0x3AC3 125 kbit/s 16 11 4 4 4 */ I am using ST library an...
Posted on May 17, 2011 at 09:36Hi, I am using MII. There are some special registers on the chip, but I guess it should work by using example from ST - but I don't try it.
Posted on May 17, 2011 at 09:36Hello! I am using Davicom DM9161AEP with Taimag RJLBC-060TC magnetics - it works, it is RoHS and I can buy it from Dacom West GmbH.
Posted on May 17, 2011 at 09:34Hello! I have got an error which is similar to the one of mjbcswitzerland My system: The board is almost like the STR912-SK from IAR - I use iSYSTEM winIDEA 2007 with iONE: the error is ''Cannot stop CPU after Startup'...