Posted on May 17, 2011 at 11:31Hi! I tried a system reset at 96Mhz. But the CPU never comes from the reset. Only after power up. In the errata sheet for STR91xF Contrioller I fond that the FMI Clock must be configured to run at 48 MHz. I have made t...
Posted on May 17, 2011 at 09:34Hello Barricade. Yes, the check of the harware-fifos works better than the check of the uart-interrupt-flags. But I have to load a File in a FPGA which has a size of 3MB, in this case I lose one or two char. The proble...
Posted on May 17, 2011 at 09:34Hello Barricade! Thanks. Your Info was my first try. With this it works much more instability. But I found something. I also use the CPU-timer-interrupt 0. It arrives every 5ms. When I disable the CPU-Timer, the UART w...
Posted on May 17, 2011 at 09:34Hello! I have a problem with the UART-Interrupt. When he arives I read the char or I write the char. Then I clear manualy the Interrupt Flag, but sometimes the Interrupt arrives immediately again and so I lose one char...
Posted on May 17, 2011 at 09:33Hi! I tried a system reset at 96Mhz. But the CPU never comes from the reset. Only after power up. In the errata sheet for STR91xF Controller I found that the FMI Clock must be configured to run at 48 MHz. I have made t...