cancel
Showing results for 
Search instead for 
Did you mean: 

System reset at 96 Mhz

heiko23
Associate II
Posted on December 05, 2006 at 06:54

System reset at 96 Mhz

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
heiko23
Associate II
Posted on May 17, 2011 at 11:31

Hi!

I tried a system reset at 96Mhz.

But the CPU never comes from the reset. Only after power up.

In the errata sheet for STR91xF Contrioller I fond that the FMI Clock must be configured to run at 48 MHz.

I have made this but the problem is still there.

Have I made somthhing wrong?

/* Enable VIC clock */

SCU_AHBPeriphClockConfig(__VIC, ENABLE);

VIC_DeInit();

SCU_RCLKDivisorConfig(SCU_RCLK_Div1); // RCLK Div 1 = 96Mhz

SCU_HCLKDivisorConfig(SCU_HCLK_Div1); // HCLK Div 1 = 96MHz

SCU_PCLKDivisorConfig(SCU_PCLK_Div1); // PCLK Div 1 = 96 MHz

SCU_FMICLKDivisorConfig(SCU_FMICLK_Div2);

FMI_Config(FMI_READ_WAIT_STATE_2, FMI_WRITE_WAIT_STATE_1,

FMI_PWD_ENABLE, FMI_LVD_ENABLE,FMI_FREQ_LOW);

SCU_PLLFactorsConfig(192,25,2); /* PLL = 96 MHz */

SCU_PLLCmd(ENABLE); /* PLL Enabled */

SCU_MCLKSourceConfig(SCU_MCLK_PLL); // Master Clock = 96 MHz

Can anyone help me?

Silicon Rev D Date Code 610

alain2399
Associate II
Posted on May 17, 2011 at 11:31

Hello

The STR9 and ST9 are different devices. Please post your question in the STR9 forum.

Regards