Posted on February 04, 2007 at 23:51Hello someone, I'm trying to get 2MHz with the internal RC oscillator of ST72264 but I don't make it work. How can I set up 2MHz with the internal RC oscillator?
Posted on October 29, 2006 at 22:39Hello, ST7LITE19B can be used for 8bit SPI master or slave. I'm trying to connect the MAX3100(SPI-UART) with ST7LITE19B. ST7 is the master, and max3100 is the slave. Max3100 requires 16bit data stream, but I cannot...
Posted on September 26, 2006 at 00:23I want a 1ms timer with ST7LITE19B. Should I use the LITE timer or the 12-bit autoreload timer? Which register should be set? and what value is needed for each control register? For example, to get 8MHZ fcpu, I s...
Posted on October 26, 2005 at 00:55Hello, I have many errors (Error: L6218E: Undefined symbol ...). How can I fix this problem? I attach my scatter file for check. Error: L6218E: Undefined symbol _Z19KC_Supply_SetStatush (referred from PWR_FAIL_ACT_...