cancel
Showing results for 
Search instead for 
Did you mean: 

Can't boot Linux with the DiskOnChip 2000 installed?

wangmowei
Associate II
Posted on September 06, 2005 at 22:47

Can't boot Linux with the DiskOnChip 2000 installed?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
wangmowei
Associate II
Posted on September 06, 2005 at 02:41

The Linux system can't boot with the DiskOnChip 2000 installed. But it can boot normally without the DOC. When the bootstrapping begins, the following error messages prompts,

Lilo

Errors 0x40

I don't know the exact reason. If you know about the error. Please help me. Thank you!

kaouther
Associate II
Posted on September 06, 2005 at 14:59

So, the problem of boot occurs only with the DOC!

Did you configured the DiskOnChip as a bootable disk for the linux?

In any case I have attached the Installation manual for the DiskOnChip2000 with Linux to verify again your configuration.

________________

Attachments :

APP21.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtsO&d=%2Fa%2F0X0000000aYE%2FhlkNmZdee00d9Y_RaMfxHzoPt5FcZVMHhNsoXZ9OWaM&asPdf=false
wangmowei
Associate II
Posted on September 06, 2005 at 22:47

Yes, perhaps it's the problem. But I can boot the linux from the DOC without CF-Card installed.

Thank you for your suggestion. I'll read the manual very carefully.