Skip to main content
luter
Associate III
March 14, 2006
Question

IAP, option bytes erasing

  • March 14, 2006
  • 1 reply
  • 716 views
Posted on March 14, 2006 at 10:47

IAP, option bytes erasing

This topic has been closed for replies.

1 reply

luter
luterAuthor
Associate III
March 14, 2006
Posted on March 14, 2006 at 10:47

Hi, All.

I'm writing bootloader for st7mc2s5t6 and i got a problem. i can not erase option bytes. steps i am doing:

1) unlock rass

2)12v on Vpp switch on

3) erasing option bytes -- operation failed :-[

I get exactly this status code after command execution.

My programming frequency is ok. all sectors are erased and flashed. i do not use readout protection. option bytes code for HDFlashEraseSector() function is 0x0f.

What is wrong?

One more thing i do not understand:

i made a loop, which executes HDFlashEraseSector() function with values range from 3 up to 255. And with some values in the range 170-180 this function returns ''Operation successful'' and option bytes are 0xff 0xff. What does it mean?

Tnx in advance.