cancel
Showing results for 
Search instead for 
Did you mean: 

programming the ST72F264 Using the ST7 IN DART

adi2
Associate II
Posted on November 17, 2003 at 09:17

programming the ST72F264 Using the ST7 IN DART

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
adi2
Associate II
Posted on November 17, 2003 at 06:19

hi !!

i'm using the ST72F264 DEMO BOARD , the in dart-stx , indart ST7 and the metrowerks as a compiler with the plug in installed.

now i'm trying to program my device but with no success, here are my steps maybe you can help me to verify what i do wrong (or did not do and need to do) :

1. i set the MCU i'm using the MCU configuration menu

2. i set the option byte

3. i load with in the indart the *.abs file

but i get errors like :

gdi-error in indart.

debugging with the metrowerks have no problams so far.

pleade advise.

thanks.

adi.

kr
Associate II
Posted on November 17, 2003 at 07:07

Are you sure that the selected clock source in the option byte is available in your application ?

adi2
Associate II
Posted on November 17, 2003 at 09:17

you are right, the clk source was not configure proper.

thanks