cancel
Showing results for 
Search instead for 
Did you mean: 

ICC Mode current consumption

clanuchnik
Associate II
Posted on June 21, 2005 at 10:46

ICC Mode current consumption

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
clanuchnik
Associate II
Posted on June 21, 2005 at 10:12

Hi,

I need to know which the typical current consumption is for the ST7LITE05 when it is running in ICC mode.

Internal RC Clock running at 8 MHZ

Thanks ..........Claudio

fggnrc
Associate II
Posted on June 21, 2005 at 10:46

Since ICC mode is activated after a reset, the power consumption would be the same of a device whose peripherals are off.

The section 13.4.1 of the ST7LITE0x datasheet (page 88) says that the max current consumption is 7 mA.

EtaPhi