Hello @Mahdouch
While waiting for the feedback from the expert, let me suggest you a further check on your setup.
STEVAL-STWINBX1 is based on STM32U5, a double-bank flash microcontroller. By default, the firmware is flashed onto the first bank. Inst...
Hello @anthonyADV
Just to confirm you that your dataset is valid and there’s no issue from the firmware side. I already found the issue on the Python SDK side and working for the solution. The error is related to the stdatalog_core wheel only. We're...
Hello @anthonyADV
Your dataset seems valid and I could convert them also if the SDK returns the error you highlighted. Have you also tried the conversion script stdatalog_examples\cli_applications\stdatalog_data_export.py?
I'm having the same error,...
Hello @anthonyADV
I'll replicate your setup locally and download the files you shared so to come back to you with more specific feedback.
Best regards,
Simone
Hello @anthonyADV
In DATALOG1, it’s the host that manages start_time and end_time parameters. DATALOG1 is compatible with the STBLESensClassic application (enabling data saving on SD card). It’s compatible also with Windows or Linux PC, enabling dat...