User Activity

Hi Everyone,I have some problems with DFU on Windows 10. I use WeAct BlackPill boards based on STM32F411 MCU. This board has BOOT0 button which allow to update firmware using STM32CubeProgrammer and DFU mode.Majority of the boards can be programmed i...
Posted on February 22, 2018 at 21:34I had some trouble with SPI before and now I have same kind of trouble with I2C. I use FreeRTOS and HAL drivers, all generated by CubeMX. Function and my fix in bold:static HAL_StatusTypeDef I2C_WaitOnRXNEFlagUnti...
Posted on December 21, 2016 at 05:41Hi,I(or may be ST) have a ptoblem. I tried to use ADC1 & ADC2 in regular dual mode with DMA on STM32F103C8T6 MCU(startup code generated by last CubeMX). If I configure ADCs in continues mode, then start ADC2(using...
Kudos from