cancel
Showing results for 
Search instead for 
Did you mean: 

When ST HAL will be fully compatible with RTOS???

Shlapunov.Nicolai
Associate II
Posted on February 22, 2018 at 21:34

I had some trouble with SPI before and now I have same kind of trouble with I2C. I use FreeRTOS and HAL drivers, all generated by CubeMX. Function and my fix in bold:

static HAL_StatusTypeDef I2C_WaitOnRXNEFlagUntilTimeout(I2C_HandleTypeDef *hi2c, uint32_t Timeout, uint32_t Tickstart)

{

  while(__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_RXNE) == RESET)

  {

   

/* Check if a NACK is detected */

    if(I2C_IsAcknowledgeFailed(hi2c, Timeout, Tickstart) != HAL_OK)

    {

      return HAL_ERROR;

    }

   

/* Check if a STOPF is detected */

    if(__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_STOPF) == SET)

    {

       // But without any received byte. ST HAL doesn't expect

       // context switching. So, if context will be switched after

       // entering into while() cycle but before STOPF check happen

       // when we receiving last byte, STOPF will be set after this

       // byte received. When context will be switched back, this

       // code will found STOPF and return an error. For prevent that,

       // after STOPF condition detected we should check RXNE bit,

       // and if we have byte - this is not an error.

       if(__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_RXNE) == RESET)

       {

         /* Clear STOP Flag */

         __HAL_I2C_CLEAR_FLAG(hi2c, I2C_FLAG_STOPF);

         /* Clear Configuration Register 2 */

         I2C_RESET_CR2(hi2c);

         hi2c->ErrorCode = HAL_I2C_ERROR_NONE;

         hi2c->State= HAL_I2C_STATE_READY;

         hi2c->Mode = HAL_I2C_MODE_NONE;

        

/* Process Unlocked */

         __HAL_UNLOCK(hi2c);

         return HAL_ERROR;

       }

    }

So, I have same kind of issue second time! Your developers should pay more attention and start thinking 'in multi-threading'.

Thanks

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0