User Activity

Posted on February 05, 2018 at 23:56Hello,I use a STM32F407 on a custom board. The application is in Motor Control. I have to read the next channels:ADC1: Channel 0 and 2ADC2: Channel 6 and 14ADC3: Channel 10 and Channel 11 and Channel 12 and Channe...
Posted on January 18, 2017 at 10:47I have a system with 1 STM32F407 and 3 STM32F401. The 407 is the master  of a communication with SPI with the 3 slaves. On the slave a use SPI in slave mode with DMA in RX/TX. On the slaves the input NSS is used in...
Posted on June 20, 2016 at 19:57Hello, I use a STM32F429 Discovery board with an other Display (Newheaven 800x480,7 incheshttp://www.newhavendisplay.com/nhd70800480efatxvctp-p-6912.htmlI use the LTDC controller of the STM32F4 to control the display....