2021-07-30 4:46 PM
Hello,
In the STM32CubeF4 project (https://github.com/STMicroelectronics/STM32CubeF4), the comment on line 42 of /Drivers/BSP/STM32412G-Discovery/stm32412g_discovery_lcd.c says that "This driver supports the LS016B8UY LCD". Then, on lines 153 to 192, the program checks for ST7789H2 and for LS016B8UY, but there is no comment concerning the ST7789H2.
Then the User Manual of the Discovery kit with STM32F412ZG MCU says (page 26) that "The display is a 1.54-inch, 240x240 pixels TFT color LCD" but the LS016B8UY seems to be a 180x180 display. So as the ST7789H2 seems to be a 240x240 display, I would rather think that the ST32412G-DISCOVERY uses the ST7789H2... but this does not match the comment.
Can you please shed some light on this?
Thank you very much in advance.
Best regards,
-- Jacques
2021-07-30 5:13 PM
Probably both at some point, what's on yours, probably going to have to look/inspect
2021-07-30 6:06 PM
Also used on L496 DISCO
1.54 inch FRD154BP2902-CTP
Lean toward SS7789H2, should be some ID registers you can read/check
2021-07-30 6:10 PM
This is the actual part https://fridalcd.en.alibaba.com/product/60667332566-800855113/1_54_inch_FRD154BP2902_full_viewing_angle_with_capacitive_touch.html
1.54 inch FRD154BP2902 full viewing angle used for smart watches
Features
No Item Specification Remark
1 Display Mode Normally Black
2 Screen Size 1.54inch
3 Resolution 240XRGBX240
4 Color Number 262K
5 Color Arrangement TFT Active matrix
6 Driver IC ST7789H2
7 Back Light White LED*3
8 Viewing Direction ALL o'clock
9 Interface MCU 8 & 16 Bit interface
10 Surface Treatment UV Cut
11 with capacitive touch panel
2021-07-31 12:53 AM
Thank you very much for your quick and detailed reply. Do you think it is worthwhile to make a pull request to also add information about the ST7789H2 in the comment ?
I would suggest replacing the following lines :
/*
1. How To use this driver:
--------------------------
- This driver is used to drive indirectly an LCD TFT.
- This driver supports the LS016B8UY LCD.
- The LS016B8UY component driver MUST be included with this driver.
*/by
/*
1. How To use this driver:
--------------------------
- This driver is used to drive indirectly an LCD TFT.
- This driver supports the ST7789H2 and LS016B8UY LCD.
- The ST7789H2 and LS016B8UY component drivers MUST be included with this driver.
*/
2021-08-06 4:23 AM
Hello @JSupc.1,
I will check and get back to you.
Chahinez.
2021-08-06 6:28 AM
Hello @JSupc.1,
The current driver is ST7789H2 adapted for RGB 240 x 240 resolution. The code has been updated to manage both old and current versions of drivers but the LCD display references are often changing unfortunately, that's why firmware are updated considering old and new material.
So, your suggest is valid. I have already reported it internally.
Thank you for your contribution.
Chahinez.
2021-08-13 1:26 PM
STM32Cube_FW_F4_V1.25.2\Drivers\BSP\Components\ls016b8uy\ls016b8uy.c
Another similar clone of the ST7789 type controller
https://cdn-shop.adafruit.com/datasheets/HX8357-D_DS_April2012.pdf
https://www.mikrocontroller.net/wikifiles/2/29/Datasheet_LDS176.pdf
https://cdn.hackaday.io/files/1660347103598656/RM68120_LCD.pdf
https://www.displayfuture.com/Display/datasheet/controller/ST7687S.pdf