2020-07-31 7:30 AM
I would like to use the STM8S005K6T6CTR in my next project. This is my first project outside of the arduino ecosystem, so sorry for bad questions(if any) .
The MCU will be responsible for taking care of the following tasks:
1) Driving a 4 digit 7 segment display
2) 4 button water tolerant capacitative touch input
3) Drive a buzzer
4) Drive a relay
5) Drive 6 LEDs
6) A timer with 1.5% accuracy(possible without external resonator?)
Thanks and Regards
2020-07-31 8:36 AM
You may want to look at stm32duino project. An arduino port for stm32 MCUs. The famous blue pill board based on stm32f103c8t6 is completely supported by stm32duino.
2020-07-31 10:02 PM
Thank You @prain . I took a look at the STM32DUINO, looks like there is support for STM8 as well. Would I still be able to use the STM's touch libraries if I were to use the stm32duino?
2020-07-31 11:50 PM
1- Until you have a good reason for using STM8 series, I strongly recommend you to use STM32. STM8 is a walking dead.
2- About touch library: depends on library; if there are dependencies on SPL, HAL, LL or any other library, you will have a hard time to port in arduino ecosystem. If it is a standalone library, it can be included in arduino projects easily. I have not experience with STM8 touch library. maybe someone else can help you better.
2020-08-01 2:11 AM
Ok. Thank you. Appreciate your reply.
2020-08-03 5:39 AM
Your tasks seem quite simple and straight forward. So I see no reason that it cannot be done with a STM8 chip.
Note that depending on the compilers used, they can have low ISR latency.