cancel
Showing results for 
Search instead for 
Did you mean: 

Where can I find the firmware for STM8S001J3

crf1000
Associate II
Posted on October 29, 2017 at 17:54

Hello,

in en.stsw-stm8069 firmware for the STM8S001J3 ist not included.

Where can i download it?

Thanks.

2 REPLIES 2
Szymon PANECKI
Senior III
Posted on October 29, 2017 at 21:58

Hello,

I have checked it and you are right that Standard Peripheral Library for STM8S doesn't include new STM8S001J3 device. It seems that libraries were not updated by us. I am sorry for this inconvenience and thank you for reporting it to us. I will provide this feedback to the team, which is responsible for these libraries.

As a temporary workaround I would recommend you to select the

STM8S003 as used device in Standard Peripheral Library. I used this approach and I didn't have any problems to control ADC, GPIOs, UART and timers of

STM8S001J3 by fuctions from Standard Peripheral Library

.

0690X00000608mgQAA.png 

Best regards

Szymon

Posted on October 31, 2017 at 23:09

Thanks a lot.