2012-01-09 1:54 AM
Please help me about
I use STM8S207 for HSI : I use UART3. I can be control it normally. with follow code -->UART3_DeInit();
UART3_Init((u32)9600, UART3_WORDLENGTH_8D, UART3_STOPBITS_1,UART3_PARITY_NO, UART3_MODE_TXRX_ENABLE);
SerialPutChar('A');
And then I change to HSE. I can not control it such as I send 'A' char to PC but PC receive only garbage char not 'A'
by I add this code -->
CLK_ClockSwitchConfig2(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSE, DISABLE, CLK_CURRENTCLOCKSTATE_DISABLE);
2012-05-19 2:07 AM
From I tried, it work if use Fosc external @24MHz, if use freq is not equal 24 MHz will be not wok.
So, we have to change a freq. of external crystal at file ''stm8s.h'' follow :#if !defined HSE_Value
#if defined (STM8S208) || defined (STM8S207) || defined (STM8AF52Ax) || defined (STM8AF62Ax)
#define HSE_VALUE ((u32)24000000) /* Value of the External oscillator in Hz*/
#else
#define HSE_VALUE ((u32)16000000) /* Value of the External oscillator in Hz*/
#endif /* STM8S208 || STM8S207 || STM8AF62Ax || STM8AF52Ax */
#endif /* HSE_Value */
By change HSE_VALUE from 24000000 to real freq. of external crystal in Hz unit