STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8L vs PIC18 code density benchmark

Posted on June 03, 2011 at 18:00Hello, I have an existing platform that I've recently built on PIC18. Soon I'm starting a new project that is very price sensitive. Currently the existing platform occupies too much code memory, avoiding me to take ...

elil by Associate III
  • 519 Views
  • 0 replies
  • 0 kudos

[resolved] GPIO: Pull-up resistors on Port E

Posted on May 21, 2011 at 15:40Hi all, I've set PE0 -> PE3 as inputs with internal pull-up enabled. Without connecting anything to these pins, I read the input register as 0x09, indicating that the pull-up is only operational on pins PE0 and PE3. Ha...

nholzem by Associate II
  • 1264 Views
  • 8 replies
  • 0 kudos

Beep function with STM8L Discovery

Posted on April 19, 2011 at 21:39Hello, I want to use the beep function with my STM8L Discovery. After writing the program to STM8L, I connect the a piezo speaker between PA0 and GND. The program is as following: // Initialize     BEEP_LSICalibratio...

PortB configured as digital Input

Posted on May 31, 2011 at 11:26Hi all, I'm trying to configure PortB as a Digital Input and afert reading the IDR register it seems to be reading the analog value of the PB0 pin. I've tried to configure PortB as PullUP no interrupt or Floating, but ...

Getting garbage over USART1

Posted on March 29, 2011 at 19:03Hi All, I have taken some of the sample code that comes with the stm8l-discovery eval board to try and talk to hyperterm on from stm8.  when i try to send anything all I see is garbage on the hyperterm screen...  I h...

mcdowell by Associate
  • 1035 Views
  • 2 replies
  • 0 kudos

SPI to communicate with an external flash memory

Posted on May 17, 2011 at 15:15Hello;I'm trying to communicate to an external flash memory (M25PE80) using SPI. I´m using the STM8SPI librarie but I´m not having success to write/read from memory. My doubt is about the configuration of pins. Are t...

STM8 core bug

Posted on April 29, 2011 at 07:56STM8 core bug

fggnrc2 by Associate II
  • 868 Views
  • 2 replies
  • 0 kudos