2022-11-01 1:01 AM
I'm using a TTC encoder connected to stm8s003f . TIM1 counts correctly until it reaches the value before the overflow value . After that it either jumps to 0 or it shows the overflow value. What is that due to?Thank you.
2022-11-01 6:57 AM
What's the maximal value of the TIM configured too? Show code.
Is the overflow just an alert, or does it have secondary consequences?
2022-11-01 11:53 PM
void Filter_Value(uint8_t value);
void clock_setup(void);
void GPIO_setup(void);
unsigned int present_value = 0x0000;
unsigned int previous_value = 0x0000;
void TIM1_setup(void);
void main(void)
{
clock_setup();
GPIO_setup();
TIM1_setup();
/* Infinite loop */
while(1){
present_value = TIM1_GetCounter()/2;
if(present_value != previous_value)
GPIO_WriteReverse(GPIOA, GPIO_PIN_1);
previous_value = present_value;
}
}
void TIM1_setup(void){
TIM1_TimeBaseInit(0, TIM1_COUNTERMODE_UP, 10, 0);
TIM1_EncoderInterfaceConfig(TIM1_ENCODERMODE_TI12, TIM1_ICPOLARITY_RISING, TIM1_ICPOLARITY_RISING);
enableInterrupts();
Filter_Value(0);
TIM1_Cmd(ENABLE);
}
void Filter_Value(uint8_t value){
TIM1->CCMR1|=(uint8_t)(value<<4);
TIM1->CCMR2|=(uint8_t)(value<<4);
}
void clock_setup(void)
{
CLK_DeInit();
CLK_HSECmd(DISABLE);
CLK_LSICmd(DISABLE);
CLK_HSICmd(ENABLE);
while(CLK_GetFlagStatus(CLK_FLAG_HSIRDY) == 0);
CLK_ClockSwitchCmd(ENABLE);
CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);
CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);
CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSI, DISABLE,
CLK_CURRENTCLOCKSTATE_ENABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_I2C, DISABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER1, ENABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_SPI, DISABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_ADC, DISABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_AWU, DISABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_UART1, DISABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER2, DISABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER4, DISABLE);
}
void GPIO_setup(void)
{
GPIO_DeInit(GPIOC);
GPIO_Init(GPIOC,
((GPIO_Pin_TypeDef)(GPIO_PIN_7 | GPIO_PIN_6)),
GPIO_MODE_IN_PU_NO_IT);
GPIO_DeInit(GPIOA);
GPIO_Init(GPIOA, GPIO_PIN_1, GPIO_MODE_OUT_PP_HIGH_SLOW);
}
2022-11-03 12:18 PM
If you read RM0016 page 185, it seems what you said, is the correct behavior.
The counter counts continuously between 0 and the auto-reload value in the TIM1_ARR register (0 to ARR or ARR down to 0 depending on the direction).