cancel
Showing results for 
Search instead for 
Did you mean: 

STVD V4.3.0 Hangs on Edit

joost
Associate
Posted on December 16, 2011 at 09:33

Hi,

My setup :

Windows Vista

STVD V4.3.0

Cosmic C compiler

STM8S Discovery board

I use the example project 'stm8s-discovery_led'. I have opened the '\Project\Discover\STVD\Cosmic\Discover.stw' workspace and it builds fine - no errors.

Whenever I try to open a source file (e.g. main.c), STVD shows the hourglass and freezes. No editor window opens, no source file is shown. The source file path that STVD shows is OK.

What am I doing wrong ?

#stvd
3 REPLIES 3
tau8051
Associate II
Posted on December 18, 2011 at 22:08

Hi , i think logging in as an administrator may solve your problem because i was having the similar kind of problem with my STVD and it was solved by logging in as administrator. (use the default administrator user)

joost
Associate
Posted on December 29, 2011 at 18:26

Hi,

I've done the install on a new PC(also Vista, no other available) and I have exactly the same problems : when trying to edit a file, STVD hangs...

It also does that when breaking in the debugger : I open the basic Discover project, send it to the debugger (without trying to edit anything). I can start the program (F5). When I then hit shift-F5 (stop and break), STVD tries to open the source file where it stopped and hangs...

I've tried every Windows trick I know (run as admin, run in XP compatibility mode, use short path names without spaces, ...) without any change. This is a very consistent bug and can not be that hard to find.

TOO BAD THERE IS NO RESPONSE FROM ST ON THIS - ABANDONING THIS MICRO - SORRY ST.

JGW.

artvolk
Associate II
Posted on December 29, 2011 at 20:55

I've the similar issue after upgrading to 4.3:

https://my.st.com/public/STe2ecommunities/mcu/Lists/STM8SDiscovery/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fSTM8SDiscovery%2fSTVD%204.3%20crashes%20on%20while%20editing%20projects%20from%204.2&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000CCDF802E596CAF44ADED5E61F5C...

You can download latest 4.2.x  -- it works. I hope that after Christmas and New Year we will have an update for the IDE...