2018-09-07 1:31 AM
The only thing which I can offer is at the end of the install when continuing from the display release notes page it hangs. I tried leaving it a while but the only way to exit is to close the program via task manager.
Any suggestions?
Thanks.
2019-05-19 7:42 AM
I have the same problem, on two different Win10 machines.
2020-04-23 8:13 AM
Any answer to this issue. i am experiencing same issue