cancel
Showing results for 
Search instead for 
Did you mean: 

STM8L151 USART not Sending, any Ideas why??

AHama.1
Associate

Hello Everyone,

This problem is persisting. I am using the STM8L151 Standard Peripheral Library to send an array of bytes over USART1. Code executes, but i see nothing on the Pin (using Oscilloscope), nor can i see the Data Rigister changing (Using ST Visual Develop, and ST Link V2 Debugger).

Can anyone see why it behaves so? -anyone made a similar ugly experience before?

thanks in advance

Here is my code inside the main:

case State_Comm_Tx:

if (State_Entrance_Part_F==0)

{

State_Entrance_Part_F=ON;

Init_USART_Tx();

//Prepare the Array to send

//uint8_t Meas_Update[6];

Meas_Update[0]= Start_Of_Text;

Meas_Update[1]= 7; // Message Length 

Meas_Update[2]=0x01; // Meassage Identifier

Meas_Update[3]= (u8) (Echo_FlyDist>>8);

Meas_Update[4]= (u8) Echo_FlyDist;

Meas_Update[5] = 0x04;

Meas_Update[6]= End_Of_Text;

USART_ClearFlag(USART1, USART_FLAG_TC);

}

if(State_Entrance_Part_F)

{

uint8_t Parameter_Nr=0;

uint8_t Tx_Array_Size= sizeof(Meas_Update);

USART_GetFlagStatus(USART1, USART_FLAG_TXE);

for(Parameter_Nr=0; Parameter_Nr< Tx_Array_Size; Parameter_Nr++)

{

while (USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET)

{}

USART_SendData8(USART1, Meas_Update[Parameter_Nr]);

}

State_Entrance_Part_F=0;

Active_State=State_Pulse_Tx;

}

break;

-------------------------------------

And the Initializsation of the USART , i do with the following function:

void Init_USART_Tx(void)

{

USART_DeInit(USART1);

CLK_PeripheralClockConfig(CLK_Peripheral_USART1,ENABLE);

USART_HalfDuplexCmd(USART1, DISABLE);

GPIO_Init(GPIOA,GPIO_Pin_2, GPIO_Mode_Out_PP_High_Fast ); // USART_Tx Pin set as output

USART_Init(USART1,115200,USART_WordLength_8b, USART_StopBits_1, USART_Parity_No, USART_Mode_Tx);

USART_Cmd(USART1,ENABLE);

}

-------------------------------------------

Thanks for your feedback

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0