STVD 3.1 errors and problems
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2012-05-24 7:28 AM
Posted on May 24, 2012 at 16:28
I'm having some problems with it. The problem is that randomly it starts to fail when you try to save any file (project, .c , . h files, etc). It happened to me 3 times already in the few days that i'm using it. One of the times one of the files was directly gone (deleted from disk) so i need to create it again (lucky that it was a .h file). I'm a bit scaried with it.
In other hand i had problems debugging, and it is not intuitive. First thing would be nice to have a direct key to program and go to debug mode (actually it doesnt have a direct key). But the most confusing and annoying stuff is that Run button (F5) restarts the program from beggining even if you stopped previously on a breakpoint..., it is the first IDE where this happens (and i'm programming since 25+ years ago). I dont see the real difference between reset and run button... i had to ''discover'' the continue button. I feel this product as something not 100% finished and i feel like a betatester :). I hope that it gets better fast since stm8s is a very interesting product
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0